2025-12-12 6:27 AM
Hello,
I'm using STM32 for a long time and really enjoy these devices to work with them.
But I'm a passionate about aviation and I want to build my own A319/A320/A321/A330 PFD/ND displays.
My idea is to use USB or Ethernet to send compressed image from X-Plane 12 to a STM32 MCU.
What I'm trying to achieve is to use a small number of devices to show the PFD image on 2 square displays of 800x800 MIPI 4 lanes.
I found some IC which can convert LTDC RGB888/RGB666/RGB565 to MIPI 4 lanes (like TC358778XBG).
My questions are:
1. There are any MCUs with dual phisical LTDC avaiable from STM? In case there is no MCU available, I will use one per display.
2. FMC can be used with SDRAM + LCD in the same time? Because I saw the physical lines are shared.
Thanks.
Solved! Go to Solution.
2025-12-13 11:59 AM
For my project I will go with something from series STM32H7 (or even STM32F7 but they have one core) with minimum of 208 pins. Everything less than this number of pins I can't activate LTDC, Ethernet, FMC and USB HS in the same time.
Thanks for the help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.