2025-10-14 12:08 AM - last edited on 2025-12-29 5:49 AM by ELABI.1
Hi everyone,
I’m working on a design using an STM32H7 MCU communicating with a GPS/GNSS module over UART. Unfortunately, during board routing, the RTS and CTS lines were connected directly (RTS↔RTS, CTS↔CTS) instead of crossed.
I understand that for proper hardware flow control, they should be:
STM32 RTS → GPS/GNSS CTS
STM32 CTS ← GPS/GNSS RTS
At this stage, I can’t modify the hardware or rework the PCB, but I’d still like to maintain some form of flow control or transmission reliability if possible.
2025-10-14 2:11 AM
Just drive them "manually" as GPIOs ?
Is XON/XOFF (so-called "software" flow control) supported?
@Muruganandam wrote:but I’d still like to maintain some form of flow control or transmission reliability if possible.
GNSS modules generally work fine without flow control ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.