2025-04-16 6:20 AM
Hello,
I'm working on LTE-M protocol and I would like to use B-L462E-CELL1 to evaluate the RF performances and characteristics of LTE-M protocol.
I would like to know, if it test tools/software to control the LTE-M chip in order to be the wanted mode is released or not?
I need this test software to program the RF device to transmit or receive mode, by defining the frenquecy and the transmit power... In order to test the following items:
- Tx Power / Frequency error
- Modulation accuracy
- Spectrum Mask
- Channel Testing
- Sensitivity
Could you please specify if this kind of control is possible and could be delivered for B-L462E-CELL1?
Thanks and Best Regards,
Asmaa
2025-04-16 7:13 AM
Welcome @Asmaa, to the community!
The LTE-M module in the B-L462E-CELL1 is from Murata, who you should contact for such special requests. However, such modules have also been discussed here in the community, e.g. here.
Hope that helps?
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.