2025-07-31 11:35 AM
Nucleo-H753ZI board. ADC1 configurations: INPUT: SINGLE-END
Sample clock rate = 5Mhz
Sample rate = 10Khz,
Sample Time = 16.5 cycles,
Resolution = 12-bit
Scan 256 times
Connect the defined two ADC input channels to GND.
The 256 readings FOR EACH INPUT are varied between (-15 - +15), more or less, while they should be read as zeros.
Question: Can it be fixed How to fix it?
Could you do the same test to confirm it?
Thanks,
Rong
2025-07-31 2:26 PM
The lowest value a single-ended ADC channel can have is 0, how do you get negative numbers?
2025-07-31 4:33 PM
Sorry, I pasted wrong data. It should be
5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10,
Total 256's. I just listed first 40's.
Thanks
2025-08-01 11:49 AM
Are you executing the calibration functions?
2025-08-01 11:55 AM
5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10, 14, 0, 0, 0, 4, 13, 0, 13, 0, 0, 0, 0, 1, 0, 0, 0, 0, 16, 8, 0, 16,12, 0, 13, 0, 0, 9, 0, 0, 0, 3, 0, 0, 15, 0, 0, 13, 0, 1, 16, 0, 0, 16, 9, 0, 0, 18, 0, 13, 0, 0, 0, 17, 0, 0, 0, 6, 0...}
2025-08-01 11:56 AM
"Are you executing the calibration functions?"
Of course.
Data
5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10, 14, 0, 0, 0, 4, 13, 0, 13, 0, 0, 0, 0, 1, 0, 0, 0, 0, 16, 8, 0, 16,12, 0, 13, 0, 0, 9, 0, 0, 0, 3, 0, 0, 15, 0, 0, 13, 0, 1, 16, 0, 0, 16, 9, 0, 0, 18, 0, 13, 0, 0, 0, 17, 0, 0, 0, 6, 0...}
2025-08-01 12:09 PM
@RongShengWang wrote:"Are you executing the calibration functions?"
Of course.
Data
5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10, 14, 0, 0, 0, 4, 13, 0, 13, 0, 0, 0, 0, 1, 0, 0, 0, 0, 16, 8, 0, 16,12, 0, 13, 0, 0, 9, 0, 0, 0, 3, 0, 0, 15, 0, 0, 13, 0, 1, 16, 0, 0, 16, 9, 0, 0, 18, 0, 13, 0, 0, 0, 17, 0, 0, 0, 6, 0...}
And to be sure we're all on the same page, how are you exactly calibrating?
2025-08-01 12:13 PM
" how are you exactly calibrating?"
2025-08-01 3:12 PM
You may need to try improving VDDA/VREFP filtering. You can also try enable oversampling.
2025-08-01 3:54 PM
What is your experience? Or you just guess? I am using Nucleo-H753ZI board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.