2025-03-25 12:57 AM
Hello, My name is Barbra, and I am working on a project using the STM32F746-DISCO board, and I need to help to debug an issue. I have written an I2C driver for the MPU6050 board, and I can't fetch any data from it. the accelerometer, gyroscope and temperature registers all seem to be at 0 always when i run the script in debug mode. I can see that the sensor gets identified through its WHO_AM_I register and gets the right readings, 0x68, but I can't get the data from the chip. i am using the STM32 HAL.
i would appreciate any help presented. Thank you.
Attatched are the files to my script.
2025-03-25 1:30 AM
@Barbra_Gitonga wrote:I can see that the sensor gets identified through its WHO_AM_I register and gets the right readings, 0x68,
Suggests that physical connections are OK, but please attach your schematic anyhow - to be sure.
@Barbra_Gitonga wrote:I can't fetch any data from it. the accelerometer, gyroscope and temperature registers all seem to be at 0 always
Have you used an oscilloscope and/or analyser on the I2C lines to see what's actually happening in the hardware?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.