2025-10-26 9:22 AM
I'm using a Blue Pill and want to replace its MCU with a genuine.one I purchased from a trusted vendor, yet I'm not 100% sure if it's actually genuine.
1- What are some of the issues with clone/copy/high copy STM32 MCUs?
2- Is there any tool/way I can check the MCU I bought with to see if it is really genuine?
Thanks in advance.
2025-10-26 9:28 AM
There is no way to check if a chip is genuine with 100% accuracy, but some things you can check are here:
Bluepill Diagnostics — Mecrisp Stellaris Unofficial 1.0 documentation
Passing the test means it may be genuine.
Failing the test means it's likely counterfeit.
2025-10-27 8:07 AM
You can ask the supplier to provide a Certificate of Conformity
2025-10-27 8:22 AM
@vernture wrote:a trusted vendor.
What vendor ?
Was it one of the Official ST Distributors?
See: https://www.st.com/content/st_com/en/contact-us.html
@vernture wrote:I'm using a Blue Pill and want to replace its MCU with a genuine..
Wouldn't it be simpler (probably also cheaper) to just buy a genuine ST board in the first place?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.