2025-06-02 1:46 PM
Hi All,
I am looking for a small 4-5 digit monochrome display to use with STM32L0 series in a coin cell powered application. Actually the display I am searching is similar to the ones used in kids watch or small temperature or humidity meters. I only need to display time or a 3 digit counter. I prefer to have wires or pins instead of the glass display with conducting rubber alignment and the length of the display should be less than 3cm. It is really hard to find even how to search for this display. It would be really great if someone can help with this.
Attaching an image as an example.
Thanks in advance,
Best regards
2025-06-02 1:50 PM
2025-06-02 2:00 PM
That was a very quick and accurate response, thanks a lot Chris. There are nice options hoping that I can fit in for my application. Length looks ok and I realized I should have also stated the width of the display. There is one option with 30x16 which I will try to fit in but if it doesn't fit, maybe I will need something with smaller width. Something like 20x12 would be the best option but I am still checking the link, there might be something close.
Thanks a lot.
2025-06-02 2:14 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.