2024-03-05 9:53 AM - edited 2024-03-05 9:54 AM
The error message I got is the following:
C:\ST\STM32CubeCLT\GNU-tools-for-STM32\bin\arm-none-eabi-gdb.exe: TUI mode is not supported
My gdb version:
GNU gdb (GNU Tools for STM32 11.3.rel1.20230912-1600) 12.1.90.20220802-git
Copyright (C) 2022 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.
Is it confirmed that this version has no TUI?
2024-03-05 1:08 PM
I can not confirm or deny. But "show configuration" in gdb will tell about compiled options. And "tui" will about tui. But maybe your system GDB is compiled with "multiarch". E.g. for SUSE is is multiarch and I do not longer need to care for the ARM gdb requiring a very special python version or crash/
2024-03-05 11:08 PM
Thanks for your reply. The command show configuration shows:
This GDB was configured as follows:
configure --host=x86_64-w64-mingw32 --target=arm-none-eabi
--with-auto-load-dir=$debugdir:$datadir/auto-load
--with-auto-load-safe-path=$debugdir:$datadir/auto-load
--with-expat
--with-gdb-datadir=/build/gnu-tools-for-stm32_11.3.rel1.20230912-1600/install-mingw/arm-none-eabi/share/gdb (relocatable)
--with-jit-reader-dir=/build/gnu-tools-for-stm32_11.3.rel1.20230912-1600/install-mingw/lib/gdb (relocatable)
--without-libunwind-ia64
--without-lzma
--without-babeltrace
--without-intel-pt
--without-mpfr
--without-xxhash
--without-python
--without-python-libdir
--without-debuginfod
--without-guile
--disable-source-highlight
--with-separate-debug-dir=/build/gnu-tools-for-stm32_11.3.rel1.20230912-1600/install-mingw/lib/debug (relocatable)
--with-system-gdbinit=/build/gnu-tools-for-stm32_11.3.rel1.20230912-1600/install-mingw/x86_64-w64-mingw32/arm-none-eabi/lib/gdbinit (relocatable)
("Relocatable" means the directory can be moved with the GDB installation
tree, and GDB will still find it.)
which suggests me that there is no python support but I cannot see anything related to the TUI. I am working on Windows 10.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.