2025-07-14 4:55 PM
Hi, I'm new to STM32 and would like to know about serial communication
via the USB port on the NUCLEO-H755ZI-Q using Arduino IDE 2.3.6.
I've already tried the program below.
As a result, the LED (PB0) blinked, but I couldn't get serial communication with the PC to work.
Could anyone let me know how I can resolve this problem?
I apologize if the information is insufficient.
void setup() {
pinMode(PB0, OUTPUT);
Serial.begin(115200);
delay(2000);
Serial.println("START");
}
void loop() {
digitalWrite(PB0, HIGH);
Serial.println("LED ON");
delay(500);
digitalWrite(PB0, LOW);
Serial.println("LED OFF");
delay(500);
}
Settings on Arduino IDE
Debug symbols and core logs: "None"
Optimize: "Smallest (-Os default)"
Board part number: "Generic H755XIHx"
C Runtime Library: "Newlib Nano (default)"
Upload method: "STM32CubeProgrammer (SWD)"
USB support (if available): "None"
U(S)ART support: "Enabled (generic 'Serial')"
USB speed (if available): "Low/Full Speed"
2025-07-14 7:14 PM
Maybe check the pins? As far as I remember, both UART and USB have more than 1 pins for the connection. On a side note, I think it would be more convenient to use STM32CubeIDE.
2025-07-17 2:30 AM
Arduino questions should go here:
https://www.stm32duino.com/ - STM32-specific
https://forum.arduino.cc/ - General Arduino
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.