2021-01-19 10:01 PM
Hi, I am new to stm32 I am not getting how to read the values what I write to the 24c16 EEPROM IC .Plz help me how to read the values by generating the read function in stm32 f103.
void write_eeprom_reg(uint16_t reg_addr, uint8_t value)
{
//uint8_t d[3];
d[0]=(reg_addr>>8) & 0xFF;
d[1]=(reg_addr) & 0xFF;
d[2]=value;
while(HAL_I2C_IsDeviceReady(&hi2c1,(uint16_t)(0x50<<1),3,100)!=HAL_OK)
{
}
if(HAL_I2C_Master_Transmit(&hi2c1,(uint16_t)(0x50<<1),(uint8_t*)d,sizeof(d),1000)!=HAL_OK)
{
Error_Handler();
}
else
{
printf("Master transmitt Successfull\r\n");
}
}
this is the code I have written for write operation but I dont know how to do code for read operation. Plz help me how to do.
Thank you
2021-01-19 10:48 PM
Use the HAL_I2C_Mem_Read and HAL_I2C_Mem_Write API functions for that.
2021-01-19 11:30 PM
Thank you. Write function is working for me but in read function I have created one buffer to store the value what I have written the value in the write function. Plz let me what mistake I have done.
uint8_t read_eeprom_reg(uint16_t addr)
{
uint8_t buf[19];
//uint8_t buffer=addr;
uint8_t value;
while(HAL_I2C_IsDeviceReady(&hi2c1,(uint16_t)(0x50<<1),3,100)!=HAL_OK)
{
}
while(HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)(0x50<<1), (uint8_t*)&buf, 2, 100)!=HAL_OK)
{
if(HAL_I2C_GetError(&hi2c1)!=HAL_I2C_ERROR_AF)
{
Error_Handler();
}
}
while(HAL_I2C_IsDeviceReady(&hi2c1,(uint16_t)(0x50<<1),3,100)!=HAL_OK)
{
}
while(HAL_I2C_Master_Receive(&hi2c1, (uint16_t)(0x50<<1),(uint8_t*)&value,1,100)!=HAL_OK)
{
if(HAL_I2C_GetError(&hi2c1)!=HAL_I2C_ERROR_AF)
{
Error_Handler();
}
return value;
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.