2020-01-19 9:08 PM
I am trying to compile directly Xcube-aws code but it's not compiling in TrueSTUDIO. In Keil it do compiled but not debug, I have to load .sfb file through uart to run code. How can I debug and merge my sensor code in Xcube-aws code and debug it. @Community member @Amel NASRI
2020-02-17 1:47 AM
Hi
I assume that you are using X-CUBE-AWS-V1.3 which uses the SBSFU as a secure Boot loader.
With SBSFU, when all security features are enabled, the DEBUG will not be possible - which is one of the protections enabled by SBSFU.
Information about the bootloader can be found in Applications/BootLoader/readme.txt.
In particular, it states that the SBSFU configuration icna be found in:
+ Configuration is located in file : ./2_Images_SBSFU/SBSFU/App/app_sfu.h
If you want to debug, you need the below lines to be uncommented:
/* Uncomment the following define when in Debug mode.
In debug mode some of the features are not activated (WRP, RDP, IWDG, DAP, etc.) */
#define SFU_DEBUG_MODE /*!< Uncomment this define when in Debug mode.
In debug mode some of the features are not activated (WRP, RDP, IWDG, DAP, etc.) */Can you please confirm that this is the case ?
Also once you've activated security features, you will need to use STM32CubeProgrammer to reset them to a non-secure state. Please read X-CUBE-SBSFU package documentation to get more information about the different setting security and how to discard them.
hope this helps
Laurent
2020-02-17 2:39 AM
Hello LMEUN,
I did uncomment that macro. Still I cannot debug my user application using stlink debugger, Is there any other way available
to debug with user application using stlink ?
Thanks and regards
swapnil
2020-02-17 3:02 AM
Hello Swapnil,
can you please confirm that you have reset your device RDP and other protections using STM32CubeProgrammer ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.