2019-11-12 10:47 PM
i think if use master and slave timer can solve this problem but i dont know required configuration in simulink
2019-11-12 11:13 PM
I don't know in simulink either, but first, read the TIM chapter in RM, and then
JW
PS Change your username to a normal nick
2019-11-12 11:22 PM
thank u;
is this setup available in stm32cubmx
2019-11-12 11:33 PM
Some TIM have N (negated) channel outputs, ie CH1 and CH1N.
Others you could use 2 channels, with one in PWM1 mode and the other in PWM2 mode, here the outputs would be the inverse of each other.
2019-11-12 11:36 PM
Maybe yes, I don't use CubeMX.
JW
2019-11-12 11:52 PM
thank u;
it seems OK;i will check it
2019-11-13 12:26 AM
you know i want two PWM that one of them has an Ts/2 delay from another, so they are not inverse of each other
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.