2016-04-22 6:02 AM
Hello,
I want to integrate the FreeRTOS and the BSP drivers in the same project for the ST32L152D-EvalBoard. I am doing my project in Atollic TrueSTUDIO and I am using the code from STM32CubeL1.Is there an easy way to do that: should I start with the FreeRTOS application and add the drivers on top, or should I start with e.g. the LCD example, and then include the FreeRTOS files?Thank you! Any idea would help me! #hal #atollic #bsp #freertosWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.