2021-01-31 12:43 PM
I have a 24FC01, 1 Kbit EEPROM on my board. The SDA and SCL lines are pulled up to 3.3V through two 2K resistors. I'm using a STM32F407 MCU to read and write data to the EEPROM. Using the HAL libraries, I'm trying to check if the device is ready using
HAL_I2C_IsDeviceReady(&i2c2, 0x50, 2, 100) function. However, this fails, returns false and triggers a hard fault. The I2C is configured in CubeMX with 100KHz clock speed and 7-bit addressing. What am I missing?
2021-01-31 2:29 PM
hello
Shift the slave address 1 bit left
0x50<<1 or 0xA0
As for the hardfault, is i2c2 a valid handler? Instead use hi2c2 used in initialization from CubeMX.
2021-01-31 9:27 PM
Oh yes, I read this but completely ignored it. Thank you. Also, yes I've been using hi2c2. This was a typo here. I'll retest and report back.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.