2019-03-03 2:15 PM
Hi all,
I have a project at Keil µVision using STM32F407VG board (it is created using cubeMX). I would export it as a plateformIO Atom project. The issue is that when generating the code in cubeMX I haven't the IDE platformIO. So I try to create a project under platformIO and I add the genrated code by cubeMX, but this did not work!!
So, can anyone help me or direct me a good tutorial for it, please.
2019-03-04 4:21 AM
Having just wasted two days myself trying to get an existing project to work under PlatformIO, are you sure this is something you really want to do ? There seem to be numerous problem in the VS Code the IDE is built upon, it seems to recompile everything on a whim so takes ages to produce code, and the upload to target throws up errors all the time. It's a good idea to have a single embedded platform but I think it hasn't matured yet, though maybe others have had more luck (or perseverance)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.