2023-02-07 11:03 PM
Could you kindly share any reference schematics for SPI EEPROM M95P32-I interfacing with STM32 MCU preferably STM32U585?
Solved! Go to Solution.
2023-02-09 7:18 AM
Hi Sreejith,
The STM32U5 has 2 types of SPI interface :
The Single SPI interface can only communicate with the M95P32-I in single SPI
This is why I suggest you to use the OctoSPI interface as it can manage single, dual, quad or Octo SPI.
In that way, you will have the flexibility to communicate with the M95P32-I in single, dual or quad SPI.
Please find attached an example of how the STM32U5 communicates with the M95P32-I
Best Regards,
Thomas
2023-02-08 5:57 AM
Hi,
Thanks for contacting our ST community support.
Which SPI modes do you want to interface with the M95P32-I ?
Single, dual or Quad SPI ?
For your information, the M95P32 Dual and Quad SPI are output only (only for reading operations)
Thanks,
Best regards,
Thomas
2023-02-08 8:36 PM
Hi Thomas,
Hope you are doing great.
In our project we will be using Single/Dual SPI and not Quad SPI.
Could you please provide reference schematics on Single/ Dual SPI of M95P32-I interfacing with STM32U585ZIT6?
Best Regards,
Sreejith
2023-02-09 7:18 AM
Hi Sreejith,
The STM32U5 has 2 types of SPI interface :
The Single SPI interface can only communicate with the M95P32-I in single SPI
This is why I suggest you to use the OctoSPI interface as it can manage single, dual, quad or Octo SPI.
In that way, you will have the flexibility to communicate with the M95P32-I in single, dual or quad SPI.
Please find attached an example of how the STM32U5 communicates with the M95P32-I
Best Regards,
Thomas
2023-02-09 8:33 PM
Hi Thomas,
Thank you for the response.
As of now we are going with single SPI. But we will consider the recommendation of choosing Quad SPI and shall revert back if I have further queries.
Thank you once again for your tremendous support.
Best Regards,
Sreejith R Nair
Professional-I
Capgemini Engineering
2023-02-09 10:19 PM
Hi Thomas,
Greetings.
Could you kindly clarify on the following point:
If we are going with single SPI interface, whether we need to use pull-up resistors for HOLD (Pin#7) and W (Write Protect, Pin#3) pins as it is mentioned in the datasheet of M95P32-I (Section 4.1) that these signals, the write protect (W) and hold (HOLD) signals must be driven high or low as appropriate. If so, please mention the pull-up resistor values.
Regards,
Sreejith
Professional I
Capgemini Engineering
2023-02-10 6:53 AM
Hi Sreejith,
You can use these resistor values :
Write protect : 4.7K
HOLD : 100K
Best Regards,
Thomas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.