2025-05-15 3:50 AM
How to flash a binary file to the microcontroller with script only ie without STM32Cube IDE & Stm32cube programmer. Please provide a detailed script to flash a given binary saved at a known location
2025-05-16 7:18 AM
Start with something simple...
Can you flash the *.bin by copying via Windows explorer to the STLINK drive?
Then doing this by *.bat?
Then build around that.
2025-05-16 7:41 AM
O boy , search somebody with basic MSDOS shell know. Dont try scripts without basic info. Flash is simple one line command batch...
"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=SWD mode=UR -d "pathto your.hex" -v -gfor bin files is required addr to load, too elf can be used instead hex usw.
read complete command help run without params
[<[start end]>] : Erase the specified sectors starting from
start code to end code, ex: -e [5 10]
-w, --write
-d, --download : Download the content of a file into device memory
<file_path> : File path name to be downloaded: (bin, hex, srec, s19
elf, stm32 or tsv file)
[<address>] : Start address of download
-w64 : Write a 64-bits data into device memory
<address> : Start address of download
<64-bit_data> : 64-bit data to be downloaded
values should not be separated by space
-w32 : Write a 32-bits data into device memory
<address> : Start address of download
<32-bit_data> : 32-bit data to be downloaded
values should be separated by space...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.