cancel
Showing results for 
Search instead for 
Did you mean: 

Are the TLV2372's surroundings and pin connections correct ?

Osman_Dag
Associate

STM32F030F4P6TR'nin PA5 pininde PWM araştırmaları. TLV2372ID ile 0-10V analog çıkış elde etmeyi planlıyorum. Devre şemasının doğru olması gerekiyor. TLV2372'nin sınırları ve pin bağlantıları doğru mu?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

English is not my native language either, but it is the language of communication defined by the community, which is why I am responding in English here.

For 0...10V, an opamp with approximately three times the gain is required (3.03, to be precise) if you have a VCC of 3.3V. According to the connection diagram, you have wired it correctly, although a drawing of opamps with a classic triangle would be clearer and better readable for the supporters here.

Please note: even though the TLV2372 is an RRIO opamp, it will output a significant output voltage of approx. 200mV at a VDD of 12V and very low input voltages close to 0.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

English is not my native language either, but it is the language of communication defined by the community, which is why I am responding in English here.

For 0...10V, an opamp with approximately three times the gain is required (3.03, to be precise) if you have a VCC of 3.3V. According to the connection diagram, you have wired it correctly, although a drawing of opamps with a classic triangle would be clearer and better readable for the supporters here.

Please note: even though the TLV2372 is an RRIO opamp, it will output a significant output voltage of approx. 200mV at a VDD of 12V and very low input voltages close to 0.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.