2026-02-25 7:40 AM
/*
* ledfunc.c
*
* Created on: Jan 16, 2026
* Author: roman
*/
#include "main.h"
#include <string.h>
#include <stdio.h>
#include "ledfunc.h"
uint8_t flag = 0;
uint8_t blue_but_click_number = 0;
char pressedKey='\0';
char readChar='\0';
//UART_HandleTypeDef huart2;
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
flag = !flag;
char main_str[50] = "Button clicked: ";
char num_str[45]; // Buffer to hold the string representation of the integer
// Convert the integer to a string
snprintf(num_str, sizeof(num_str), "%d times\r\n", ++blue_but_click_number);
// Concatenate the new string to the main string
// You must ensure main_str has enough allocated space for both parts
strncat(main_str, num_str, sizeof(main_str) - strlen(main_str) - 1);
HAL_UART_Transmit(&huart2, (uint8_t*)main_str, strlen(main_str), HAL_MAX_DELAY);
char msg[20];
sprintf(msg, "PRESSED: %c\r\n", pressedKey); // Formats string + char
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), 100);
}
void ledblibk(int blinknum) {
for (int i = 0; i < blinknum; i++) {
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
leddelay(500);
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
leddelay(500);
}
}
void leddelay(int ms) {
SysTick->LOAD = 16000 - 1;
SysTick->VAL = 0;
SysTick->CTRL = 0x5;
for (int i = 0; i < ms; i++) {
while (!(SysTick->CTRL & 0x10000)) {
}
}
SysTick->CTRL = 0;
}
void ledblink() {
if (1 == flag) {
HAL_GPIO_TogglePin( LD2_GPIO_Port, LD2_Pin);
HAL_Delay(50);
} else {
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
}
}
char Keypad_Read(void) {
char keypad_map[4][4] = {
{'1','2','3','A'},
{'4','5','6','B'},
{'7','8','9','C'},
{'*','0','#','D'}
};
for (int i = 0; i < 4; i++) {
// 1. Set current row to LOW (assuming Row pins are PC0-PC3)
HAL_GPIO_WritePin(GPIOC, (GPIO_PIN_0 << i), GPIO_PIN_RESET);
// 2. Check each column (assuming Column pins are PC4-PC7)
for (int j = 0; j < 4; j++) {
if (HAL_GPIO_ReadPin(GPIOC, (GPIO_PIN_4 << j)) == GPIO_PIN_RESET) {
while(HAL_GPIO_ReadPin(GPIOC, (GPIO_PIN_4 << j)) == GPIO_PIN_RESET); // Debounce/Wait for release
HAL_GPIO_WritePin(GPIOC, (GPIO_PIN_0 << i), GPIO_PIN_SET); // Reset row before returning
return keypad_map[i][j];
}
}
// 3. Set row back to HIGH
HAL_GPIO_WritePin(GPIOC, (GPIO_PIN_0 << i), GPIO_PIN_SET);
}
return 0; // No key pressed
}Hello all
I learn ( code below) !!!
Blue button is on EXTI - works. When press LED2 blinks, press again - LED stops blink ( work as expected)
Press on Blue button also sends message ( debugging purposes ) to Serial comm 9600 ( works as expected )
Now I added Keypad_Read() function to read pressed key ( this doesn't work ) Please advice me on getting
keypad only
connected 4x4 keypad as below
My code below
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2026 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
#include "ledfunc.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim3;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_TIM3_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_TIM3_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1) {
ledblink();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief TIM3 Initialization Function
* @PAram None
* @retval None
*/
static void MX_TIM3_Init(void)
{
/* USER CODE BEGIN TIM3_Init 0 */
/* USER CODE END TIM3_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM3_Init 1 */
/* USER CODE END TIM3_Init 1 */
htim3.Instance = TIM3;
htim3.Init.Prescaler = 999;
htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
htim3.Init.Period = 499;
htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM3_Init 2 */
HAL_TIM_Base_Start_IT(&htim3);
HAL_TIM_Base_Start(&htim3);
/* USER CODE END TIM3_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 9600;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : B1_Pin */
GPIO_InitStruct.Pin = B1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : PC0 PC1 PC2 PC3 */
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pin : LD2_Pin */
GPIO_InitStruct.Pin = LD2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : PC4 PC5 PC6 PC7 */
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) {
if (htim == &htim3) {
//HAL_GPIO_TogglePin( LD2_GPIO_Port, LD2_Pin);
pressedKey=Keypad_Read() ;
}
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1) {
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */and
/*
* ledfunc.c
*
* Created on: Jan 16, 2026
* Author: roman
*/
#include "main.h"
#include <string.h>
#include <stdio.h>
#include "ledfunc.h"
uint8_t flag = 0;
uint8_t blue_but_click_number = 0;
char pressedKey='\0';
char readChar='\0';
//UART_HandleTypeDef huart2;
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
flag = !flag;
char main_str[50] = "Button clicked: ";
char num_str[45]; // Buffer to hold the string representation of the integer
// Convert the integer to a string
snprintf(num_str, sizeof(num_str), "%d times\r\n", ++blue_but_click_number);
// Concatenate the new string to the main string
// You must ensure main_str has enough allocated space for both parts
strncat(main_str, num_str, sizeof(main_str) - strlen(main_str) - 1);
HAL_UART_Transmit(&huart2, (uint8_t*)main_str, strlen(main_str), HAL_MAX_DELAY);
char msg[20];
sprintf(msg, "PRESSED: %c\r\n", pressedKey); // Formats string + char
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), 100);
}
void ledblibk(int blinknum) {
for (int i = 0; i < blinknum; i++) {
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
leddelay(500);
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
leddelay(500);
}
}
void leddelay(int ms) {
SysTick->LOAD = 16000 - 1;
SysTick->VAL = 0;
SysTick->CTRL = 0x5;
for (int i = 0; i < ms; i++) {
while (!(SysTick->CTRL & 0x10000)) {
}
}
SysTick->CTRL = 0;
}
void ledblink() {
if (1 == flag) {
HAL_GPIO_TogglePin( LD2_GPIO_Port, LD2_Pin);
HAL_Delay(50);
} else {
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
}
}
char Keypad_Read(void) {
char keypad_map[4][4] = {
{'1','2','3','A'},
{'4','5','6','B'},
{'7','8','9','C'},
{'*','0','#','D'}
};
for (int i = 0; i < 4; i++) {
// 1. Set current row to LOW (assuming Row pins are PC0-PC3)
HAL_GPIO_WritePin(GPIOC, (GPIO_PIN_0 << i), GPIO_PIN_RESET);
// 2. Check each column (assuming Column pins are PC4-PC7)
for (int j = 0; j < 4; j++) {
if (HAL_GPIO_ReadPin(GPIOC, (GPIO_PIN_4 << j)) == GPIO_PIN_RESET) {
while(HAL_GPIO_ReadPin(GPIOC, (GPIO_PIN_4 << j)) == GPIO_PIN_RESET); // Debounce/Wait for release
HAL_GPIO_WritePin(GPIOC, (GPIO_PIN_0 << i), GPIO_PIN_SET); // Reset row before returning
return keypad_map[i][j];
}
}
// 3. Set row back to HIGH
HAL_GPIO_WritePin(GPIOC, (GPIO_PIN_0 << i), GPIO_PIN_SET);
}
return 0; // No key pressed
}
2026-02-25 12:11 PM
Thank you @mƎALLEm
This code is just a draft - just to see board led+but+usart in action
2026-02-25 12:14 PM - edited 2026-02-25 11:33 PM
Even if it's a draft it induces issues. You need to keep interrupts execution as short as possible while printf stretches the execution and blocks the interrupt for awhile.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.