2007-08-01 10:20 PM
WIU and falling edge triggered interrupts
2011-05-17 12:45 AM
This is my first post so I'm hoping someone can help or point me in the right direction!
I have a Hitex ARM STR912 Starter Kit and IAR compiler. The starter kit has 5 push button switches (which are high when released and low when pressed) which I've configured to generate a VIC1.9 (WIU all) interrupt. The interrupts are configured for falling edge. In the interrupt service routine for the WIU I've added a simple count++ statement. The problem I get is this:- When I press a button, I get an interrupt as expected and 'count' increments. When I release the button I also get an interrupt and 'count' is incremented a second time. We've scoped the switch input and it looks pretty clean when released. Whats interesting is if I set the interrupt trigger to rising edge, pushing and releasing the button only generates the one interrupt and it behaves as expected. Anyone got any thoughts?2011-05-17 12:45 AM
Thanks mirou
I'm using the VIC1.9 (WIU all) as the interrupt source. Will have to do a bit more investigation.2011-05-17 12:45 AM
Hello GoSquirrels,
I've tested a code as you described it and I didn't face any problem with WIU interrupt. I work with IAR compiler on the STR9 Eval-Board. You find attached the IAR project. Are you using another interrupt with WIU interrupt? With best regards, mirouWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.