2007-08-01 8:06 PM
2011-05-17 12:45 AM
Hello,
I yet have made a Remote frame. The object is declared as CAN_SetRxMsgObj(Remote_Frame,....); If I receive the remote frame in the interrupt the object will be changed to transmit. This is done automatically from the STR9-Can with the receive of a RTR-Bit. Then I send on the same object (proper a receive object) the reply-message. The automatical reply of the remote frame doesn't work, because I have to toggle a bit in the reply-frame. Good luck2011-05-17 12:45 AM
Hello,
I have to send remote frame on the CAN Bus with the ST library (CAN_SendMessage function). How can i do that ? Regards ArnoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.