2018-09-24 3:46 AM
Dear All,
I am using STM8L ...
I had tried ST library functions to write option bytes but they aren't written.
the code as following :-
halt_opt_byte = FLASH_ReadByte(0x4808);
if( halt_opt_byte != 0x02 )
{
FLASH_ProgramOptionByte(0x4808, 0x02);
}
Still option byte is equal to Zero.
void FLASH_ProgramOptionByte(uint16_t Address, uint8_t Data)
{
/* Check parameter */
assert_param(IS_OPTION_BYTE_ADDRESS(Address));
/* Enable write access to option bytes */
FLASH->CR2 |= FLASH_CR2_OPT;
/* Program option byte and his complement */
*((PointerAttr uint8_t*)Address) = Data;
FLASH_WaitForLastOperation(FLASH_MemType_Program);
/* Disable write access to option bytes */
FLASH->CR2 &= (uint8_t)(~FLASH_CR2_OPT);
}
Thanks a lot,
Ahmed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.