2005-01-05 10:24 PM
Why I cannot shift >> 12 an integer???
2005-01-03 3:52 AM
When I do:
Tempvalue = (Value>>12); the link generate: ERROR M5108: Called application detected an error project.prm with: #pragma DATA_SEG DEFAULT extern unsigned int Tempvalue; extern unsigned int Value; Same error if i do: Value = TEmpvalue / 1000; Thanks a lot2005-01-05 1:09 AM
hi marchino,
I got no pb at all, here is the code generated: 48 int_value1 = int_value2 >> 12; 0xfaf1 LD Y,#0x0c 0xfaf4 LD A,int_value2+1 0xfaf7 LD X,int_value2 0xfafa CALL _ILSR 0xfafd LD int_value1+1,A 0xfb00 LD int_value1,X The Hiware compiler is using a function of thelibrary _ILSR to prform the shift. I just used the default setting for compiler and linker provided by STVD7 R3.1.1 Best regards2005-01-05 10:24 PM
Hi marchino,
the error message seams to come from the maker of your Metrowerks environment. More details you'l find in the maker manual, that you can download from metrowerks underhttp://ftp://ftp.metrowerks.com/pub/docs/Targets/HC08_CW08_3.0/Maker.pdf
Proably there is no access to the ansi library Rtsst7.c or it is corrupted. Regards WoRoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.