2019-04-11 2:51 AM
I downloaded and installed the COSMIC stm8 free compiler (http://cosmicsoftware.com/download_stm8_free.php).
I requested and received a license.
I copied the license file to the appropriate folder.
However, the compiler does not start.
It does not start from ST Visual Develop.
I tried to run it on the command line, from the folder in which it is located (D:\Program Files\COSMIC\FSE_Compilers\CXSTM8).
I see error: "D:\Program Files\COSMIC\FSE_Compilers\CXSTM8\cxstm8.exe not a valid Win32 application"
I use Windows XP SP3.
I tried 3 times reinstall compiler. And i got same error.
2019-04-11 3:28 AM
Cosmic has it's own user forum, and promises installation support. Have you tried it there ?
Not much seasoned STM8/Cosmic users present here.
2019-04-11 9:35 AM
No, I have not tried it yet.
The file Readme.txt says "If you have any question, please post them on: https://my.st.com/public/STe2ecommunities/mcu/default.aspx or send e-mail to support.stm8.free@cosmic.fr".
And so I wrote here.
Do not tell me a link to the COSMIC forum?
2019-04-20 2:27 PM
I am looking at my Project settings and it looks like it automatically set the path to C:\Program Files(x86)\COSMIC\FSE_Compilers\CXSTM8 - try to install everything with default paths.
You can also try to ensure that in your project settings the path is correct.
2019-04-21 11:55 PM
Thanks for the help.
I wrote to the support team and they told me that their compiler no longer supports running on Windows XP.
Nothing can be done about it.
The topic is closed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.