2023-05-31 2:40 AM
If I commented these lines again error is notified in Clk.c file and repeated for other.
My question is, if commenting all those lines will reflect any issues in building the code
2023-05-31 2:53 AM
I'm not familiar with the code lines in question, but the error suggests you're missing an include file or define. Perhaps address those issues rather than simply commenting out the lines?
2023-05-31 4:11 AM
i haven't written any code just created a workspace included library files and compiled .Its showing me error in the library files.
assert_param(IS_ADC1_CONVERSIONMODE_OK(ADC1_ConversionMode));
assert_param(IS_ADC1_CHANNEL_OK(ADC1_Channel));
assert_param(IS_ADC1_PRESSEL_OK(ADC1_PrescalerSelection));
assert_param(IS_ADC1_EXTTRIG_OK(ADC1_ExtTrigger));
assert_param(IS_FUNCTIONALSTATE_OK(((ADC1_ExtTriggerState))));
assert_param(IS_ADC1_ALIGN_OK(ADC1_Align));
assert_param(IS_ADC1_SCHMITTTRIG_OK(ADC1_SchmittTriggerChannel));
assert_param(IS_FUNCTIONALSTATE_OK(ADC1_SchmittTriggerState));
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.