cancel
Showing results for 
Search instead for 
Did you mean: 

What is GPIO_IPInputConnected_Enable ?

s_bhujbal
Associate II
Posted on October 13, 2009 at 18:34

What is GPIO_IPInputConnected_Enable ?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
s_bhujbal
Associate II
Posted on May 17, 2011 at 09:58

Dear All,

Can anybody tell me, what is use of GPIO_IPInputConnected_Enable ?

When this to be enable or disable ?

Does it mean if a pin is Input Function pin then above property of pin should be enable or if it is Output Function pin then above property should be disabled ?

Suppose I initialised a pin for any output function & I enabled ''IPInputConnected'' property for the same pin, then can I read the status of that pin by library function ?

Please clearify me if anybody knows it .

Regards,

Sachin Bhujbal

lillian_200601
Associate II
Posted on May 17, 2011 at 09:58

I have the same understanding as s_bhujbal. Any one can clarify it for us?

Thanks

tomas23
Associate II
Posted on May 17, 2011 at 09:58

Nope, IPInputEnabled connects the pin with the peripheral Alternate Function inputs. Imagine UART Rx as an example.

The standard GPIO doesn't need this option enabled.

See Fig. 28 in RefMan and pin allocation table in Datasheet.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.