2023-07-19 1:10 AM
Hi Experts.
I have a project that requires a circuit design using VN5T006ASP-E and VND5T016ASP-E. The temperature of use is -40°C to 85°C. The VN5T006ASP-E needs to pass a continuous current of 10A, and the VND5T016ASP-E needs to pass a current of 5A on each of the two channels, can this be achieved? As shown in the figure below, the manual does not give a specific labeling of how much current can be passed.What is the maximum current that can be passed by VN5T006ASP-E and VND5T016ASP-E? Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.