2011-11-22 7:17 AM
hello, I'm trying to trigger the ADC1 with the TRGO signal of TIM1, here is the code that I,m using to configure the timer:
TIM1_DeInit(); TIM1_TimeBaseInit(128, TIM1_CounterMode_Up, 62500, 0); TIM1_SelectOutputTrigger(TIM1_TRGOSource_Update); TIM1_Cmd(ENABLE); while for configuring the ADC1 and getting the conversion result I'm using (adapted from STM8L-discovery firmware): u16 ADC_CH3_TRIG(void) { uint8_t i; uint16_t res; /* Enable ADC clock */ CLK_PeripheralClockConfig(CLK_Peripheral_ADC1, ENABLE); /* de-initialize ADC */ ADC_DeInit(ADC1); /*ADC configuration ADC configured as follow: - Channel 3 - Mode = Single ConversionMode(ContinuousConvMode disabled) - Resolution = 12Bit - Prescaler = /1 - sampling time 9 */ ADC_Cmd(ADC1, ENABLE); ADC_Init(ADC1, ADC_ConversionMode_Single, ADC_Resolution_12Bit, ADC_Prescaler_1); ADC_SamplingTimeConfig(ADC1, ADC_Group_FastChannels, ADC_SamplingTime_9Cycles); ADC_ExternalTrigConfig(ADC1, ADC_ExtEventSelection_Trigger2, ADC_ExtTRGSensitivity_Rising); ADC_ChannelCmd(ADC1, ADC_Channel_3, ENABLE); delay_10us(3); /* initialize result */ res = 0; for(i=8; i>0; i--) { /* start ADC convertion by software */ //ADC_SoftwareStartConv(ADC1); /* wait until end-of-covertion */ while( ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == 0 ); /* read ADC convertion result */ res += ADC_GetConversionValue(ADC1); } /* de-initialize ADC */ //ADC_VrefintCmd(DISABLE); ADC_DeInit(ADC1); /* disable SchmittTrigger for ADC_Channel_24, to save power */ //ADC_SchmittTriggerConfig(ADC1, ADC_Channel_24, DISABLE); CLK_PeripheralClockConfig(CLK_Peripheral_ADC1, DISABLE); ADC_ChannelCmd(ADC1, ADC_Channel_3, DISABLE); return (res>>3); } The program seems to hang up at the while loop waiting for EOC signal... what am I doing wrong? Is there an application note that I can use for ADC triggering with a timer? #adc-stm82012-03-13 5:39 AM
STM8L15x standard peripheral library 1.5.1
In this library, you can see ADC_DMA example. I hope this will help. Regards,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.