2019-09-09 7:47 AM
Hi,
I am trying to design a power supply using eDesignSuite, having universal input from85~265VAC/50Hz and having 1 isolated output 10V@15mA and two non-isolated outputs 15V@75mA and 3.3V@50mA (flyback converter). But I am unable to design both isolated and non-isolated outputs in eDesignSuite.
Could you please help me in this regard?
Best Regards,
Anayat
Solved! Go to Solution.
2019-09-09 8:18 AM
eDesignSuite allows you to design AC/DC isolated and not isolated flyback converters with VIPerx6 and VIPerx1 ICS.
For VIPerx6 solutions, you can even specify more than one output.
Best regards,
Patrizia
2019-09-09 7:54 AM
Hello,
sorry but this kind of solution cannot be directly designed through eDesignSuite.
Best regards,
Patrizia
2019-09-09 7:57 AM
2019-09-09 8:11 AM
You can surely use VIPerx6 or VIPerx1 family ICs.
2019-09-09 8:14 AM
2019-09-09 8:18 AM
eDesignSuite allows you to design AC/DC isolated and not isolated flyback converters with VIPerx6 and VIPerx1 ICS.
For VIPerx6 solutions, you can even specify more than one output.
Best regards,
Patrizia
2019-09-09 8:22 AM
2019-09-09 8:32 AM
Yes, either isolated or non isolated designs
2019-09-09 8:33 AM
2019-09-09 8:36 AM
You're welcome.
Best regards,
Patrizia
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.