2006-02-07 6:25 PM
2006-02-02 6:50 AM
Hello All,
I am using STR711F and done with enumeration as HID device. I am using IAR Kickstart board. I am simultaneously developing (sort of reusing) a small host side application to talk with the device. Whenever I write on endpoint, it always writes on control endpoint and I get USB monitor trafic as: 000001: Class-Specific Request (DOWN), 02.02.2006 13:56:59.3556808 +67.5633648 Destination: Inrterface, Index 0 Reserved Bits: 34 Request: 0x9 Value: 0x201 Send 0x11 bytes to the device 01 04 43 72 05 30 30 30 30 30 30 30 30 30 00 00 00..Cr.000000000... 000002: Control Transfer (UP), 02.02.2006 13:56:59.3556808 +0.0 Pipe Handle: 0x84685020 Setup Packet 21 09 01 02 00 00 11 00 !....... Recipient: Inrterface Request Type: Class Direction: Host->Device Request: 0x9 (Unknown) Value: 0x201 Index: 0x0 Length: 0x11 The problem is, it always writes on control endpoint. I am using the same host side application which I am using for one of my previous USB projects with ATMEL AT89C5132. And it works with that and writes on Endpoint 2 (0x02). Can anybody tell me what may be wrong in host side application? My question might not be related to this forum but any help will be appreciated. Thanks in advance, Ranga [ This message was edited by: ranga on 02-02-2006 20:22 ] UPDATE: Problem is solved. My HID report was correct but I didn't enable the OUT endpoint and that's why the host was writting on Endpoint 0. Anyways thanks for reading.[ This message was edited by: ranga on 02-02-2006 22:32 ]2006-02-07 6:25 PM
Can you describe your USB definitions?
report descriptor device descriptor etc.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.