2006-03-09 1:05 AM
2006-03-08 10:36 PM
Hi to all,
i'm starting to create a firmware to control USB pheripheral of STR710 uC, but I have some problem about descriptor structure creation. I ask you to provide some documentaion about my problem; USB Software Library don't explain this problem solution. Thanks to all,2006-03-09 12:23 AM
/******************** (C) COPYRIGHT 2003 STMicroelectronics ********************
* File Name : usb_desc.c * Author : MCD Application Team * Date First Issued : 27/10/2003 * Description : Descriptors for USB Mouse * ********************************************************************************/ #include ''USB_lib.h'' #include ''USB_desc.h'' const BYTE MOUSE_ReportDescriptor[MOUSE_SIZ_REPORT_DESC] = { 0x05, /* Usage Page(Generic Desktop) */ 0x01, 0x09, /* Usage(Mouse) */ 0x02, 0xA1, /* Collection(Logical) */ 0x01, 0x09, /* Usage(Pointer) */ 0x01, /* 8 */ 0xA1, /* Collection(Linked) */ 0x00, 0x05, /* Usage Page(Buttons) */ 0x09, 0x19, /* Usage Minimum(1) */ 0x01, 0x29, /* Usage Maximum(3) */ 0x03, /* 16 */ 0x15, /* Logical Minimum(0) */ 0x00, 0x25, /* Logical Maximum(1) */ 0x01, 0x95, /* Report Count(3) */ 0x03, 0x75, /* Report Size(1) */ 0x01, /* 24 */ 0x81, /* Input(Variable) */ 0x02, 0x95, /* Report Count(1) */ 0x01, 0x75, /* Report Size(5) */ 0x05, 0x81, /* Input(Constant,Array) */ 0x01, /* 32 */ 0x05, /* Usage Page(Generic Desktop) */ 0x01, 0x09, /* Usage(X axis) */ 0x30, 0x09, /* Usage(Y axis) */ 0x31, 0x09, /* Usage(Wheel) */ 0x38, /* 40 */ 0x15, /* Logical Minimum(-127) */ 0x81, 0x25, /* Logical Maximum(127) */ 0x7F, 0x75, /* Report Size(8) */ 0x08, 0x95, /* Report Count(3) */ 0x03, /* 48 */ 0x81, /* Input(Variable, Relative) */ 0x06, 0xC0, /* End Collection */ 0x09, 0x3c, 0x05, 0xff, 0x09, /* 56 */ 0x01, 0x15, 0x00, 0x25, 0x01, 0x75, 0x01, 0x95, /* 64 */ 0x02, 0xb1, 0x22, 0x75, 0x06, 0x95, 0x01, 0xb1, /* 72 */ 0x01, 0xc0 }; /* MOUSE_ReportDescriptor */ const BYTE MOUSE_DeviceDescriptor[MOUSE_SIZ_DEVICE_DESC] = { /* ST mouse */ 0x12, /* bLength */ 0x01, /* bDescriptorType */ 0x00, /* bcdUSB */ 0x01, 0x00, /* bDeviceClass */ 0x00, /* bDeviceSubClass */ 0x00, /* bDeviceProtocol */ 0x08, /* bMaxPacketSize0 */ 0x83, /* idVendor (1155) */ 0x04, 0x01, /* idProduct */ 0x00, 0x04, /* bcdDevice rel. 1.04 */ 0x01, 4, /* Index of string descriptor */ /* describing manufacturer */ 42, /* Index of string descriptor */ /* describing product */ 0, /*98,*/ /* Index of string descriptor */ /* describing the device's */ /* serial number */ 0x01 /* bNumConfigurations */ }; /* MOUSE_DeviceDescriptor */ const BYTE MOUSE_ConfigDescriptor[MOUSE_SIZ_CONFIG_DESC] = { 0x09, /* bLength: Configuation Descriptor size */ 0x02, /* bDescriptorType: Configuration */ MOUSE_SIZ_CONFIG_DESC, /* wTotalLength: Bytes returned */ 0x00, 0x01, /* bNumInterfaces: 1 interface */ 0x01, /* bConfigurationValue: */ /* Configuration value */ 0x00, /* iConfiguration: */ /* Index of string descriptor */ /* describing the configuration */ 0xA0, /* bmAttributes: */ /* bus powered, remote-wakeup */ 0x32, /* MaxPower 100 mA: this current is used for detecting Vbus */ /******************** Descriptor of mouse interface ********************/ /* 09 */ 0x09, /* bLength: Interface Descriptor size */ 0x04, /* bDescriptorType: */ /* Interface descriptor type */ 0x00, /* bInterfaceNumber: Number of Interface */ 0x00, /* bAlternateSetting: Alternate setting */ 0x01, /* bNumEndpoints*/ 0x03, /* bInterfaceClass: HID */ 0x01, /* bInterfaceSubClass : 1=BOOT, 0=no boot*/ 0x02, /* nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse*/ 0, /* iInterface: */ /* Index of string descriptor */ /******************** Descriptor of Mouse HID ********************/ /* 18 */ 0x09, /* bLength: HID Descriptor size */ 0x21, /* bDescriptorType: HID */ 0x00, /* bcdHID: HID Class Spec release number */ 0x01, 0x00, /* bCountryCode: Hardware target country */ 0x01, /* bNumDescriptors: */ /* Number of HID class descriptors */ /* to follow */ 0x22, /* bDescriptorType */ MOUSE_SIZ_REPORT_DESC, /* wItemLength: Total length of Report descriptor */ 0x00, /******************** Descriptor of mouse endpoint ********************/ /* 27 */ 0x07, /* bLength: Endpoint Descriptor size */ 0x05, /* bDescriptorType: */ /* Endpoint descriptor type */ 0x81, /* bEndpointAddress: */ /* Endpoint Address (IN) */ 0x03, /* bmAttributes: Interrupt endpoint */ 0x04, /* wMaxPacketSize: 4 Byte max */ 0x00, 0x20, /* bInterval: Polling Interval (32 ms) */ /* 34 */ }; /* MOUSE_ConfigDescriptor */ const BYTE MOUSE_StringDescriptor[MOUSE_SIZ_STRING_DESC] = { 0x04, 0x03, 0x09, 0x04, /* LangID = 0x0409: U.S. English */ /* 4 */ 38, /* Size of manufaturer string */ 0x03, /* bDescriptorType = String descriptor */ /* Manufacturer: ''STMicroelectronics'' */ 'S',0, 'T',0, 'M',0, 'i',0, 'c',0, 'r',0, 'o',0, 'e',0, 'l',0, 'e',0, 'c',0, 't',0, 'r',0, 'o',0, 'n',0, 'i',0, 'c',0, 's',0, /* 42 */ 56, 0x03, /* Product name: ''ARM7 : USB Mouse Tutorial'' */ 'A',0, 'R',0, 'M',0, '7',0, ' ',0, ' ',0, ' ',0, ':',0, ' ',0, 'U',0, 'S',0, 'B',0, ' ',0, 'M',0, 'o',0, 'u',0, 's',0, 'e',0, ' ',0, 'T',0, 'u',0, 't',0, 'o',0, 'r',0, 'i',0, 'a',0, 'l',0, /* 98 */ 28, 0x03, /* Serial number: ''20072000-0001'' */ '2',0, '0',0, '0',0, '7',0, '2',0, '0',0, '0',0, '0',0, '-',0, '0',0, '0',0, '0',0, '1',0, /* 126 */ 26, 0x03, /* Interface 0: ''ST USB Mouse'' */ 'S',0, 'T',0, ' ',0, 'U',0, 'S',0, 'B',0, ' ',0, 'M',0, 'o',0, 'u',0, 's',0, 'e',0, /* 152 */ }; /* MOUSE_StringDescriptor */2006-03-09 1:05 AM
Hi Bassof
http://www.beyondlogic.org/usbnutshell/usb5.htm#DeviceDescriptors
page might help you. regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.