2017-10-09 5:18 AM
I’m trying to understand STM8 pipelining to be able to predict how much cycles my code will need.
(I alreadyhttps://stackoverflow.com/questions/46629607/understanding-stm8-pipelining
, but I figured this focum is probably the better audience).I have this example, where I toggle a GPIO pin for 4 cycles each. Iffloopis aligned at 4byte-boundary + 3, the pin stays active for 5 cycles (i.e. one more than it should). I wonder why?
// Switches port D2, 5 cycles high, 4 cycles low void main(void) { __asm bset 0x5011, #2 ; output mode bset 0x5012, #2 ; push-pull bset 0x5013, #2 ; fast switching jra _loop .bndry 4 nop nop nop _loop: nop bset 0x500f, #2 nop nop nop bres 0x500f, #2 jra _loop __endasm; }
A bit more context:
So in cycles:
According to this, the pin should stay LOW for 4 cycles and HIGH for 4 cycles, but it’s staying HIGH for 5 cycles.
In any other alignment case, the pin is LOW/HIGH for 4 cycles as expected.
I think, if the PIN stays high for an extra cycle that must mean that the execution pipeline is stalled after thebsetinstruction (thenops thereafter provide enough time to make sure thatbreslater is ready to execute immediately). But according to my understandingnop(for 6.) would already be fetched in 4.
Any idea how this behavior can be explained? I couldn’t find any hints in the
. #cpu #cycle #pipelining #performanceWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.