2009-08-17 3:03 AM
2011-05-17 12:59 AM
There appears to have been a bug introduced to the uIP main loop in the application note/example um0238 from ST. This bug is not in the original uIP 0.9 source code.
The problem is the line: if (size > 0) uip_len = size; This should be: uip_len = size; Otherwise, if some non-IP and non-ARP packet is recieved (i.e. another type of ethernet data), then uip_len is set greater than zero, but not cleared until an IP or ARP packet is recieved. http://en.wikipedia.org/wiki/Ethertype An alternative fix would be to have: else { uip_len = 0; } if both 'if (BUF->type==...' checks fail.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.