2009-10-13 8:16 AM
STR9 as I2C 10-bit Master transmitter
2011-05-17 12:59 AM
Hi all,
I'm implementing on STR91 I2C communication with an I2C EEPROM. The initialisation was done and I can send addresses and data to EEPROM but only in 7-bit Master transmitter/receiver mode. Now I would like to use 10-bit Master transmitter/receiver mode but I can't find any information how to initialise I2C on STR91 in 10-bit mode. In 10-bit Master mode STR91 have to send first a Header and after EV9 the Address. It sounds simple, but I never get the EV9 event and ADD10 bit is never set. On my mind Header contains device code, 3 MSBits of address and R/W flag. Or I'm wrong? Perhaps someone can help me to solve this problem. Thanks! Best Regards Ivunin2011-05-17 12:59 AM
Do you send a proper first address byte? Its format is 11110xxS, where XX are 8- and 9-th bits, S is R/\W. Read Philips I2C spec on the net, chapters 14 and 14.1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.