2010-06-22 11:47 PM
UART1 example with reference to chm file(stm8s_fwlib_um)
2011-05-17 6:09 AM
Hi ,
Regarding the reference manual the BRR values are evaluated using fMaster = 24Mhz and in your case you have fMaster = 16MHz. Can you please check another hypertherminal tool (try Hercules.exe) and your hardware connection. You can download Hercules.exe from this link: http://hercules-setup.hw-group-s-r-o.qarchive.org/ If the Hypertherminal is not correctly configured you should receive data but is not correct. The expected data ''HyperTerminal Interrupt: UART1-Hyperterminal communication using Interrupt'' Best Regards mozraWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.