Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Set Option Bytes AFR, STM8S207RB

Hello Everyone,I am to test a device which uses the STM8S207RB as the controller. The controller's pin 25 and 26 are used for I2C communication. But in order to use it for the SDA and SCL signals, I need to remap its function by changing the AFR6 bit...

huck lim by Associate
  • 1353 Views
  • 1 replies
  • 0 kudos

Stm8s003f3 Pin as SPI MOSI and use MISO as GPIO

1. I am using Stm8s003f3.In it a slave SPI device is connected, which only inputs data, it dont output any data so MOSI is only used.2. My question is can I use remianing MISO pin as GPIO? since MOSI is used after configuring SPI, will it automatcial...

I would like to know how to use any timer, say TIM2, and GetCounter() correctly. I'm using SDCC on linux and compiling for an STM8L051. Please see some example blinky code. Below is the code I think should work. Any help is greatly appreciated.

void main(void) { uint16_t tmpcnt = 0; uint8_t tmpcntrl, tmpcntrh;   setup_pins();   CLK_PeripheralClockConfig(CLK_Peripheral_TIM2, ENABLE); TIM2->PSCR = TIM2_Prescaler_1; TIM2->ARRH = 0; TIM2->ARRL = 1; TIM2->CNTRH = ...

AClap.1 by Associate II
  • 1958 Views
  • 3 replies
  • 0 kudos

STM8S005K6 I2C Bus always busy

Hi.Regarding I2C Bus busy problem. I am using alternative pins (PB4 and PB5), as I have the small chip with fewer pins.Option bits are set, and verified.However even at power up the BUSY bit is set. It is set through configuration of the I2C peripher...

HMoel.1 by Associate II
  • 1311 Views
  • 1 replies
  • 0 kudos

Why is the Halt() function not working?

#include <stm8l15x.h> #include <stm8l15x_pwr.h>   void main(void) { GPIO_Init(GPIOA, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); GPIO_Init(GPIOB, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); GPIO_Init(GPIOC, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); ...

TheUser by Associate II
  • 4348 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.