2008-09-30 10:02 AM
UART1 DMA Not working, HW problem
2011-05-17 12:55 AM
Hi
I tried using UART1 with DMA If I have a gap between characters longer than a character width I get garbage characters in the DMA Buffer If I use UART0 all is well You can see this on a scope, I sent the scope & ICE displays previously Is ST Micro going to fix this?2011-05-17 12:55 AM
What is your setup code? do you have the fifo enabled on UART1?
2011-05-17 12:55 AM
Everything was setup the same
All I did was change the UART from 1 to 0 and DMA Receive started working properly There is a HW bug in the silicon For Receive I have a gap of several character times & I get trash in the UART1 FIFO Uart1 rECEIVE does stop at the proper number of real characters, BUT I now have trash in the FIFOWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.