2008-12-09 1:01 AM
2011-05-17 12:56 AM
Hi all,
I am not getting(Received data)data Via UART0 when both UART0 and UART2 are enabled(all Initialisation is done properly).When I have commented UART2 initialisation then I am able to receive data via UART0.UART0 Tx works in both conditions. UART0 Pin(Port 6.6(Rx),6.7(Tx)) UART2 Pin(Port 3.0(Tx),3.1(Rx)) How can use both Please guide me through Regard Sai2011-05-17 12:56 AM
You have to be careful using pins 3.0 and 3.1 for UART2 because they can also be used for UART0. Misconfiguring something can cause some headache as it's not immediately obvious what's going wrong since the code compiles and runs without any other trouble.
What is the code you use to initialize the pins for UART0 and UART2?2011-05-17 12:56 AM
Hi all
UART0 configuration is as follows: void Init_UART0(unsigned long l_ulg_BaudRate) { GPIO_InitTypeDef GPIO_InitStructure; UART_InitTypeDef UART_InitStructure; SCU_APBPeriphClockConfig(__UART0, ENABLE); SCU_APBPeriphReset(__UART0, DISABLE); SCU_APBPeriphClockConfig(__GPIO6 , ENABLE); SCU_APBPeriphReset(__GPIO6, DISABLE); //UART0 Rx pin configuration GPIO_InitStructure.GPIO_Direction = GPIO_PinInput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable; GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1; GPIO_Init (GPIO6, &GPIO_InitStructure); //UART0 Tx pin configuration GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt3; GPIO_Init (GPIO6, &GPIO_InitStructure); //UART0 Configuration UART_InitStructure.UART_WordLength = UART_WordLength_8D; UART_InitStructure.UART_BaudRate = l_ulg_BaudRate; UART_InitStructure.UART_StopBits = UART_StopBits_1; UART_InitStructure.UART_Parity = UART_Parity_No ; UART_InitStructure.UART_HardwareFlowControl = UART_HardwareFlowControl_None; UART_InitStructure.UART_Mode = UART_Mode_Tx_Rx; UART_InitStructure.UART_FIFO = UART_FIFO_Disable; UART_Init(UART0, &UART_InitStructure); VIC1->VAiR[1] = (u32)UART0_IRQHandler; VIC1->VCiR[1] = 0x20 | 0; VIC1->INTSR &= ~(1); VIC1->INTER |= (1); UART_ITConfig(UART0,UART_IT_Receive, ENABLE); //Enable Receive Interrupt UART_Cmd(UART0, ENABLE); //Enable UART0 } UART2 configuration is as follows: void Init_UART2(unsigned long l_ulg_BaudRate) { GPIO_InitTypeDef GPIO_InitStructure; UART_InitTypeDef UART_InitStructure; SCU_APBPeriphClockConfig(__UART2, ENABLE); SCU_APBPeriphReset(__UART2, DISABLE); SCU_APBPeriphClockConfig(__GPIO3 , ENABLE); SCU_APBPeriphReset(__GPIO3, DISABLE); //UART0 Rx pin configuration GPIO_InitStructure.GPIO_Direction = GPIO_PinInput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable; GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1; GPIO_Init (GPIO3, &GPIO_InitStructure); GPIO_StructInit(&GPIO_InitStructure); //Reset GPIO initstructure //UART0 Tx pin configuration GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init (GPIO3, &GPIO_InitStructure); //UART0 Configuration UART_InitStructure.UART_WordLength = UART_WordLength_8D; UART_InitStructure.UART_BaudRate = l_ulg_BaudRate; UART_InitStructure.UART_StopBits = UART_StopBits_1; UART_InitStructure.UART_Parity = UART_Parity_No ; UART_InitStructure.UART_HardwareFlowControl = UART_HardwareFlowControl_None; UART_InitStructure.UART_Mode = UART_Mode_Tx_Rx; UART_InitStructure.UART_FIFO = UART_FIFO_Disable; UART_Init(UART2, &UART_InitStructure); UART_Cmd(UART2, ENABLE); //Enable UART0 } Let me know if I have done any mistake Regards Sai2011-05-17 12:56 AM
When I configure my UARTs, for the Tx GPIO pins, I have:
GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable; Somewhat counter-intuitive, but it's been working for me so I guess it's worth a shot.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.