2021-03-01 2:08 AM
Hi,
I am using stm8s105c6 for UART transmit receive program. I am using Eclipse with SDCC compiler.
I am getting error as
?ASlink-Warning-Undefined Global '_TIM3_CAP_COM_IRQHandler' referenced by module 'main'
make: *** [main] Error 1
Hope someone will guide me.
Thanks in advance
2021-03-01 2:28 AM
You seem to call a function that does not exist in your project.
2021-03-01 2:43 AM
Thanks Ozone.
Please see program,
#include "stm8s.h"
#include <stdio.h>
#include "stm8s_uart2.h"
#include "gpio.h"
#include "stm8s_gpio.h"
#include "stm8s_clk.h"
#include "stm8s_it.h"
void main(void){
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
GPIO_DeInit(GPIOD);
/* Configure PD5/6 */
GPIO_Init (UART2_TX__PORT, UART2_TX__PIN, GPIO_MODE_OUT_PP_HIGH_FAST); // send data IO
GPIO_Init (UART2_RX__PORT, UART2_RX__PIN, GPIO_MODE_IN_FL_NO_IT); // accept data IO
UART2_DeInit();
UART2_Init((uint32_t)115200,UART2_WORDLENGTH_8D,UART2_STOPBITS_1,UART2_PARITY_NO,UART2_SYNCMODE_CLOCK_DISABLE,UART2_MODE_TXRX_ENABLE); //Baud rate 2400 8-bit data
UART2_ITConfig (UART2_IT_RXNE_OR, ENABLE); // agree to accept the interrupt
UART2_ITConfig(UART2_IT_TXE, ENABLE);
UART2_Cmd (ENABLE); // enable serial port
enableInterrupts(); //Open total interrupt
while(1){
}
}
and I am getting errors are:
?ASlink-Warning-Undefined Global '_CLK_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_EXTI_PORTA_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_EXTI_PORTB_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_EXTI_PORTC_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_EXTI_PORTD_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_EXTI_PORTE_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TLI_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_SPI_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TIM2_UPD_OVF_BRK_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_AWU_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TIM3_UPD_OVF_BRK_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TIM4_UPD_OVF_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_EEPROM_EEC_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TRAP_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TIM1_UPD_OVF_TRG_BRK_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_UART2_RX_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_UART2_TX_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_ADC1_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_I2C_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TIM1_CAP_COM_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TIM2_CAP_COM_IRQHandler' referenced by module 'main'
?ASlink-Warning-Undefined Global '_TIM3_CAP_COM_IRQHandler' referenced by module 'main'
make: *** [main] Error 1
D:\ash_eclipse_workspace_2\uart>ren main.ihx main.hex
I hope you could guide me further.
2021-03-25 12:52 AM
Looks like you are using some library (SPL, I guess), and including the header files for it, but not linking the library into your binary. I think you are just missing some -l option to your linker command.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.