2007-11-28 12:43 AM
Uart starts missing BYTEs and/or Packet when TIM0 Enabled
2011-05-17 12:48 AM
Hi,
My application use UART0 and a Timer (time base of 1ms) with the STR9. When I disable timer interrupt, everything is fine with the UART. When I enable the Timer, some packet are OK and randomly, it stops working. Something it looks like I receive the last TX that I've done. I tried to use instead of the TIM0 (that has a bigger interrupt level than the UART) to use Periodical RTC (that has a lower interrupt level than the UART), but without success. My UART settings are: SCU_APBPeriphClockConfig(__UART0, ENABLE) SCU_APBPeriphReset(__UART0,DISBLE) UART_InitStructure.UART_WordLength = UART_WordLength_8D; UART_InitStructure.UART_StopBits = UART_StopBits_1; UART_InitStructure.UART_Parity = UART_Parity_No ; UART_InitStructure.UART_BaudRate = 9600; UART_InitStructure.UART_HardwareFlowControl = UART_HardwareFlowControl_None; UART_InitStructure.UART_Mode = UART_Mode_Tx_Rx; UART_InitStructure.UART_FIFO = UART_FIFO_Disable; UART_DeInit(UART0) UART_ITConfig(UART0,UART_IT_Transmit,DISABLE) UART_ITConfig(UART0, UART_IT_Receive,ENABLE) VIC_Config(UART0_ITLine, VIC_IRQ,5) VIC_ITCmd(UART0_ITLine,ENABLE) UART_Init(UART0,&UART_InitStructure) UART_Cmd(UART0,ENABLE); My TIM0 Settings are : SCU_APBPeriphClockConfig(__TIM01, ENABLE) SCU_APBPeriphReset(__TIM01,DISBLE) TIM_DeInit(TIM0) VIC_Config(TIM0_ITLine, VIC_IRQ, 6) VIC_ITCmd(TIM0_ITLine, ENABLE) freq = SCU_GetPCLKFreqValue() Tmr0_Cmp_Value = freq / TMR0_PRESCALER) TIM0->OC1R = Tmr0_Cmp_Value TIM_PrescalerConfig(TIM0, (TMR0_PRESCALER – 1)) TIM_CounterCmd(TIM0,TIM_START) TIM_ITConfig(TIM0, TIM_IT_OC1, ENABLE) My Alternative config of the RTC is: SCU_APBPeriphClockConfig(__RTC, ENABLE) SCU_APBPeriphReset(__RTC,DISBLE) RTC_DeInit() RTC_PeriodicIntConfig(RTC_Per_1024Hz); VIC_Config(RTC_ITLine, VIC_IRQ, 6) VIC_ITCmd(RTC_ITLine, ENABLE) RTC_ITConfig(RTC_IT_Per, ENABLE)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.