2021-03-18 12:16 AM
I am using stm8s105c6 discovery board. I want to generate timer 1 interrupt and toggle led. But I am not able to generate timer interrupt.
void delay_cycles(uint16_t cy)
{
do{
--cy;
}while(cy);
}
//void TIM1_UPD_OVF_TRG_BRK_IRQHandler(void)
void TIM1_CAP_COM_IRQHandler(void)
{
GPIO_WriteHigh(GPIOB, GPIO_PIN_6);
if(flag == 0){
flag = 1;
// GPIO_WriteHigh(GPIOB, GPIO_PIN_4);
}
//TIM1_ClearITPendingBit(TIM1_IT_UPDATE);
TIM1_ClearITPendingBit(TIM1_IT_CC4);
TIM1_ARRPreloadConfig(ENABLE);
}
void main (void)
{
// CLK_DeInit();
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_UART2, ENABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, ENABLE);
GPIO_DeInit(GPIOC);
GPIO_DeInit(GPIOB);
GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_OUT_PP_LOW_FAST); //PC4 CHANNEL 4 TIMER1
GPIO_Init(GPIOB, GPIO_PIN_6, GPIO_MODE_OUT_PP_LOW_FAST); //GPIO
TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_DOWN,4095, 0); //timer freq = (clock CPU/16) -> 1bit = 1uS -> 92*1uS=92uS
TIM1_OC4Init(TIM1_OCMODE_PWM2,TIM1_OUTPUTSTATE_ENABLE,2047,
TIM1_OCPOLARITY_HIGH, TIM1_OCIDLESTATE_SET);
TIM1_CtrlPWMOutputs(ENABLE);
TIM1_ITConfig(TIM1_IT_UPDATE, ENABLE);
// TIM1_ITConfig(TIM1_IT_CC4, ENABLE);
TIM1_Cmd(ENABLE);
// GPIO_WriteHigh(GPIOD,GPIO_PIN_6);
GPIO_WriteHigh(GPIOB,GPIO_PIN_6);
GPIO_WriteLow(GPIOB,GPIO_PIN_6);
enableInterrupts();
while(1) {
if(flag == 1){
flag = 0;
}
}
please guide me.
thanks in advance
}
2021-03-20 2:18 AM
You enable the interrupt on UPDATE
TIM1_ITConfig(TIM1_IT_UPDATE, ENABLE);
// TIM1_ITConfig(TIM1_IT_CC4, ENABLE);but the interrupt routine is on CAPTURE COMPARE
void TIM1_CAP_COM_IRQHandler(void)
{
GPIO_WriteHigh(GPIOB, GPIO_PIN_6);
if(flag == 0)
{
flag = 1;
}
TIM1_ClearITPendingBit(TIM1_IT_CC4);
TIM1_ARRPreloadConfig(ENABLE);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.