2009-03-03 12:46 AM
2011-05-17 12:57 AM
Hello,
I'm using the STR-9 processor and have a requirement to ''sync'' one of the internal timers to an external GPS 1PPS input. Any suggestions on how best to accomplish this task using the STR-9 micro? Thanks :D2011-05-17 12:57 AM
Hi,
According to the lack of details in your 1st post, maybe you could describe a little bit more, What do you mean by ''sync on GPS signal'' (I never worked with GPS signal). Do you want to start to count a duration on a edge, or count the number of pulse or somethings else. Keep me in touch. Regards. Damien hoyen2011-05-17 12:57 AM
Hi Damien,
Thanks for your reply. We have a GPS module receiving several satellites and this module outputs a precise 1PPS signal as a very accurate time sync pulse at about 50ms. What I need to do is sync with this 1PPS to generate a 1 minute Frame signal and within that Frame, allocate 2250 slots at 26.67ms each slot. I will then output a 37.49Hz square wave timing signal for other circuits. This project is a TDMA (time division multiple access) signaling system. Thanks for any suggestions, Alan :DWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.