2011-02-02 1:24 AM
Timer 2 - One pulse mode
2011-05-17 6:11 AM
please ensure you have not erroneously set option bit ADC_ETR [AFR0].
brazov2011-05-17 6:11 AM
Hi brazov,
Thanks for your response. I haven't touch this option byte. This is my code for TIM3.Code with TIM3:
TIM3_DeInit();
TIM3_TimeBaseInit(0,150);
TIM3_OC2Init(TIM3_OCMODE_PWM1,TIM3_OUTPUTSTATE_ENABLE,1,TIM3_OCPOLARITY_HIGH);
TIM3_ICInit(TIM3_CHANNEL_1,TIM3_ICPOLARITY_RISING,TIM3_ICSELECTION_INDIRECTTI,0,0);
/* TIM3_CCxCmd */
TIM3->CCER1 |= (u8)TIM3_CCER1_CC1E;
/* TIM3_SelectOnePulseMode */
TIM3->CR1 |= (u8)TIM3_CR1_OPM;/* TIM3_Cmd */
TIM3->CR1 |= (u8)TIM3_CR1_CEN;
Regards.
Sly
2011-05-17 6:11 AM
is it TIMER2 or TIMER3 .... anyway:
// *** TIMER 2 INITIALIZATION ***
TIM2->CCMR1= 1 & TIM1_CCMR_CCxS; // IC1 input is mapped on TI1FP1
TIM2->SMCR|= (5<<4) & TIM2_SMCR_TS; // edge on TI1FP1 will make a TRGI
TIM2->SMCR|= (6<<0) & TIM2_SMCR_SMS; // trigger mode (counter starts at rising edge of the TRGI)
TIM2->SMCR|= (1<<7) & TIM2_SMCR_MSM; // enable master slave mode
TIM2->CCR2H= (u8)(OUTPCOMPARE >> 8); // init pulse wide - compare register
TIM2->CCR2L= (u8)(OUTPCOMPARE);
TIM2->ARRH= (u8)(AUTORELOAD >> 8); // init auto reload register
TIM2->ARRL= (u8)(AUTORELOAD);
repet= REPETITION; // repetition counter setting
TIM2->RCR= repet-1;
TIM2->EGR= TIM2_EGR_UG; // update registers
TIM2->CCMR2= (7<<4) & TIM2_CCMR_OCM | TIM2_CCMR_OCxPE; // OC2PWM 2 output compare mode
TIM2->CCER2= TIM2_CCER2_CC2E; // OC2 enable output pin
TIM2->BKR|= TIM2_BKR_AOE; // automatic enable outputs
TIM2->CR1|= TIM2_CR1_OPM; // one pulse mode
TIM2->CR1|= TIM2_CR1_CEN; // TIM2 enable
2011-05-17 6:11 AM
yes, you're right I was able to do it only with TIM1 see Reference Manual pag.173. Is there someone who succedded in doing it with TIM2/TIM3?
brazov2011-05-17 6:11 AM
So your code is unusable.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.