Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
void PWM(void)//timer1 channel4{ TIM1_ARRH = 0x03; // Reload counter = 960TIM1_ARRL = 0xc0;TIM1_PSCRH|= 0; // Prescalar = 0 (i.e. 1)TIM1_PSCRL |= 0;//TIM1_CR1 = 0; // Up counter.TIM1_CR1|= 0; // Edge aligned counter.TIM1_RCR |= 0; /...
I am getting the error i posted below , while i build the program.Anyone know how to solve this error.Please respond , It is urgent.///////////////////////////////////////////////////////////////////////////////////////////////////////////////Running...
Not able to install PSDsoft tools on windows 10 machine. So that we are unable to download application into uPSD3234A with Keil and ULIKN2. ULINK2 was able to detect the target but debug settings are asking for PSDsoft project file(filename.ini). Cou...
Hi,We have been using the M24128 EEPROM IC on our access control products to store user data.I have attached the schematic of the chip below. There are 1k ohms pull ups to 3.3V on the SDA and SCL lines which are not shown in the image.Recently we fou...
We can assume that it is surrounded by room temperature air.
I can't find any example programs for continuous mode. Well I found one but it doesn't even have a makefile to run it on my microcontroller.
I would like to use the STM8S005K6T6CTR in my next project. This is my first project outside of the arduino ecosystem, so sorry for bad questions(if any) .The MCU will be responsible for taking care of the following tasks:1) Driving a 4 digit 7 segm...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.