2010-06-29 8:08 AM
Time controlled by timer
2011-05-17 6:09 AM
Hi moussa,
Probably you have a non-coherence between stm8s_it.c, stm8s.it_h and interrupt_vector.c. Why you are not using the template provided by ST in the standard library. It is easier and faster for start-up ? That was my case when I started enjoying with STM8S micros. Tell me if It is OK now. Regards, MCU Lüfter2011-05-17 6:09 AM
Hi lowpowermcu,
finally i succeeded to generate the interruption and the time is controled perfectly thanks to your help,
thank you very much,now i want to communicate with stp08dp05 driver leds via SPI communication,
in ST web site i thought AN2478 application but it's developed with ST7lite, have you any ideas to program with stm8 thank you so much Best regards,2011-05-17 6:09 AM
Hi moussa,
I didn't used it but you can start with the provided examples on SPI and then to update it to your requirement. If you have some news thanks to share. With regards, MCU Lüfter2011-05-17 6:09 AM
Hello Chnani,
I am also having a problem similar to you. That is in my case also the timer counter is not getting increased. But going through the thread I cant understand what changes have helped you to overcome the problem. So can you please tell me explicitly which registers were changed and what are the values that gave you the desired output? Thank you.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.