cancel
Showing results for 
Search instead for 
Did you mean: 

TDA7566

Raj23
Associate

We are working on one of our project which previously using TDA7566 IC.

Can anyone suggest any pin-to-pin compatible IC for TDA7566?

Are the following IC's are compatible - TDA7580, TDA7388, TDA7850?

I would like to know more about the 3 pins (pin number: 22, 25, 4) of TDA7566 as there are mainly 3 pins which are not match with TDA7384A & TDA7385 and similar case with other IC's.

 

 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Raj23, to the community!

As you may have seen, the TDA7566 has been discontinued for a long time. Pins 22, 25 and 4 in question provided functions that are unfortunately no longer included in any other class AB amp still available: I2C Clock/Data and CD_Out (Clip Detector Output). These pins are used by all the alternatives as MUTE, DIAGNOSTICS and ST-BY.

I'm sorry, but apart from remaining stocks of the TDA7566, which you may find somewhere on the Internet, I can't give you a pin2pin compatible alternative if your project uses the pins mentioned.

Regards
/Peter


In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.