Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
I need some technical materials about this wifi module and some tutorials about receiving data. I'm working about simple application who works like that:1) The sensor measures temperature and sends data through UART interface. Next this information i...
Hi,I'm using stm8s003f3p6 microcontroller and learn it's different internal peripheral. using SPLHow can i write a byte at RAM location like 0x00 and read from it.i also want to use IAP commands for flash.i have read stm8s Reference manual , dastashe...
We have a programming problem for this ST CHN P 24C32WP K2A823 component that was provided to us. The reference component we use and know how to program is the ST CHN P 24C32WP K2A237. The only difference in marking on the IC is 823 instead of 237. W...
Posted on November 13, 2009 at 05:51Dummy question : .axf size greater than Flash size???
Good day!I'm using STVD+Cosmic. How do I set up the variable in the RAM at the specific position.I've tried creating new Segment and Section but the variable is declared at another address in the flash.Also, nothing changes when I'm changing min or m...
Hi all.I would to flash a .hex firmware into some STLUX385A devices.These devices are not brand new and de optionbytes allowing serial bootloader has been removed by previous application. Worst-case scenario, the serial pins are not accessible on the...
Hi.I want to read the EEPROM but i don't see any function for this. i write my data in eeprom by hal_flashex_dataeeprom_program() function and i want transmit eeprom's data with uart to pc. how can i do this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.