2003-10-01 11:15 PM
2003-10-01 8:17 PM
hi! all
I have some problems about TBU timer... it's my function. pragma TRAP_PROC SAVE_REG void timer1() { //unsigned char i; //unsigned char key_temp; //unsigned char key_temp1; // timer decrement //if(ValBit(TBUCSR, 5)) // { if(t_hdd) t_hdd--; // } if(t_fan) t_fan--; if(t_audio) t_audio--; if(t_printer) t_printer--; if(t_cd) t_cd--; if(t_ad) t_ad--; if(t_adint) t_adint--; // time base 1sec if(tb_100ms) tb_100ms--; else { tb_100ms = 10; if(t_disp) t_disp--; } // time base 1sec if(tb_1sec) tb_1sec--; else { tb_1sec = 100; t_1sec++; } // key input chattering routine //unsigned char keytemp; //unsigned char keytemp1; sela(0); selb(1); key_temp = PBDR; asm ld A, PBDR asm ld key_temp, A key_temp = PBDR; //key_temp = key_temp & 0x01; asm LD A, key_temp asm AND A,0x01 asm LD key_temp,A key_temp = key_temp << 2; key_temp1 = key_temp; sela(1); selb(0); //key_temp = PBDR; asm ld A, PBDR asm ld key_temp, A //key_temp = key_temp & 0x01; asm LD A, key_temp asm AND A,0x01 asm LD key_temp,A key_temp = key_temp << 1; key_temp1 = key_temp1 + key_temp; sela(0); selb(0); //key_temp = PBDR; asm ld A, PBDR asm ld key_temp, A //key_temp = key_temp & 0x01; asm LD A, key_temp asm AND A,0x01 asm LD key_temp,A key_temp1 = key_temp1 | key_temp; i = key_temp1; //i = _pa; //i &= 0x07; // || ((_pc & 0x0 << 1) & 0x10); if(i == key_buffer) { if(key_count) key_count--; else { key_data = i; key_count = 6; } } else { key_buffer = i; key_count = 6; } } I set timer1's vector in prm file, and set TBUCSR, and TBUCV register, I have questions now... 1)Interrupt was not enable without ''asm RIM'' instruction why? is it another way to enable inturrupt? 2)this function steps at debugging mode. when function is over, it is back to first of function ''if(t_hdd)'' everytime Idon't know why. can I fix it? [ This message was edited by: JayB on 02-10-2003 08:48 ]2003-10-01 9:30 PM
1.) RIM is an global interrupt enable instruction . You can not have the timer interrupt without enabling the global interrupt bit.
2.) Try to run it continuosly. It returns again to the the function due to the pending interrupt.2003-10-01 11:15 PM
thanks for your help!
I don't want to be back to timer function every time... I want to be back in period time, I set tbu registers, but It returns every time. how can I do?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.