2013-03-04 12:14 PM
Was using STVD successfully for a couple of projects on two different machines. One machine is still working fine.
I cannot create a new project targeting either the Raisonance Tool Chain, or any other tool chain (assembly only included) because in all cases, the MCU Selection List is Empty. Have reinstalled versions 4.3.1 and 4.3.3 several times. I can compile with Raisonance using an old project where the MCU is still selected, but cannot link because the -P option for rlstm8 is not present (the -P option is there on the machine that works, and without it, the Raisonance linker complains about the demo period being over). I have noticed that after reinstalling, all my recent lists are still present in the ide as well as several other options selected while running. I'm guessing that the inability to load the mcu list is related to not completely reinstalling the IDE from scratch so if anyone knows how to clean a system from all files related to STVD, please help me out. Have tried cleaning the registry of all things related to STVD, but no luck. Latest installer log : Setup launched on 3-4-2013 at 13:51:58 Script version not found: ignored First setup mode Platform 5.1 - intel processor Processing password: standard tools ExecMachineName=Version 4.3.1 PATH modified for ASM toolchain parport service stopped: no driver installed for parallel port Launched ''C:\Program Files\STMicroelectronics\st_toolset\stvp\STTubDriver\STTSLink_Install.bat MFC redistribution not necessary (already present). Setup ends successfully #stvd2013-03-06 7:17 AM
Machine A (still working) install log :
Setup launched on 7-6-2012 at 14:41:58 Script version not found: ignored First setup mode Platform 5.1 - intel processor Processing password: standard tools ExecMachineName=Version 4.3.1 PATH modified for ASM toolchain parport service stopped: no driver installed for parallel port Launched ''C:\Program Files\STMicroelectronics\st_toolset\stvp\STTubDriver\STTSLink_Install.bat Redistributing MFC 4053 MFC redistribution done. Setup ends successfullyMachine B (stopped working) install log :
Setup launched on 3-5-2013 at 12:49:04 Script version not found: ignored First setup mode Platform 5.1 - intel processor Processing password: standard tools ExecMachineName=Version 4.3.3 parport service stopped: no driver installed for parallel port Launched ''C:\Program Files\STMicroelectronics\st_toolset\stvp\STTubDriver\STTSLink_Install.bat MFC redistribution not necessary (already present). Setup ends successfullyMachine C (never worked) install log :
Setup launched on 3-5-2013 at 20:18:15 Script version not found: ignored First setup mode Platform 5.1 - intel processor Processing password: standard tools ExecMachineName=Version 4.3.3 PATH modified for ASM toolchain parport service stopped: no driver installed for parallel port Launched ''C:\Program Files\STMicroelectronics\st_toolset\stvp\STTubDriver\STTSLink_Install.bat Redistributing MFC 4053 MFC redistribution done. Setup ends successfully
2013-03-06 9:02 AM
A possible clue :
on machines that don't work, stvdebug.exe is using : msvcp80.dll Microsoft C++ Runtime Library Microsoft Corporation 8.0.50727.6195 msvcr80.dll Microsoft C Runtime Library Microsoft Corporation 8.0.50727.6195 and on machine that does, stvdebug.exe is using : MSVCP80.dll Microsoft C++ Runtime Library Microsoft Corporation 8.0.50727.4053 MSVCP90.dll Microsoft C++ Runtime Library Microsoft Corporation 9.0.30729.4974 MSVCR80.dll Microsoft C Runtime Library Microsoft Corporation 8.0.50727.4053 MSVCR90.dll Microsoft C Runtime Library Microsoft Corporation 9.0.30729.4974 So possibly a 4053 vs 6195 issue?2013-03-06 12:03 PM
So for devilment, I pulled the 6195 versioned dlls off the machine that didn't work hoping it would revert to the 4053 versions. Tried without a fresh uninstall/reinstall, and it wouldn't run at all (still looking for the 6195 versions), uninstalled, then reinstalled, and although install was successful, it still wouldn't run until I replaced the 6195 dlls. There must be something that ties stvdebug.exe to the 6195 versions during install that is skipped on subsequent installs.
Oh well, spent much too much time on this already so I tried out a nearby Win8 machine. Seems to not have the same problem, so I'll come out better buying a new machine than spending another couple of days trying to figure this out.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.