2004-10-28 2:16 AM
STVD 3.0.1 and Cosmic Floating Point Libraries
2004-10-27 3:39 AM
Having a problem getting floating point libraries to work with STVD7. In the Cosmic manual, it says to link the floating point library first, i.e
libfs.st7 libis.st7 libm.st7 However, STVD 3.0.1 puts the floating point library last in the linker file: libis.st7 libm.st7 libfs.st7 I am not 100% sure this is the cause yet, but should this go on the wish list?2004-10-27 9:56 PM
2004-10-28 2:16 AM
Hi MD,
I just made the test with stvd7 3.0.1 I created a new workspace and project with Cosmic toolset, selected short stack model as you in the compiler settings tab and checked the float lib in the linker tab (input category). As you can see in the following extracted lines, the generated lkf files (in debug and release subdirectories) respect the right order as specified in the Cosmic manual... # libfs.st7 libis.st7 libm.st7 # Are you sure you didn't modified manually this file ? Please check in the project settings linker tab (input category) that you still have the Auto button checked. Emmanuel.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.